FTM0 PWM Stop at PTB0, PTB1 GPIO work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FTM0 PWM Stop at PTB0, PTB1 GPIO work

1,775 Views
franksdyang
Contributor I

When PTB0, PTB1 don't be set, FTM0 PWM don't work.
and when input pulses in GPIO mode are put to PTB0, FTM0 stops.
When PTB0, PTB1 are set to GPIO and no input pulse, FTM0 work.
FTM0 symtom is really abnormal.

What is the problem?

MCU: MK10DN32VLF5

Compiler: IAR EWARM ver 6.5

Code is below:

<Initialization>

/* FTM0 ----------------------------------------------------------------- */
    SIM_SCGC6 |= SIM_SCGC6_FTM0_MASK;

/* PTC2(Pin 35) PWM_TO_DAC */
    PORTC_PCR2 &= ~PORT_PCR_MUX_MASK;
    PORTC_PCR2 |= PORT_PCR_MUX(4);   // FTM0_CH1

/* Write Protection Disable */
    FTM0_MODE |= FTM_MODE_WPDIS_MASK;
    /* FTM Enable */
    FTM0_MODE |= FTM_MODE_FTMEN_MASK;
   
    /* Counter run in BDM mode */
    /* FTM Counter Functional mode */
    FTM0_CONF |= FTM_CONF_BDMMODE(3);
   
    /* Set PWM frequency; MODULO = Fclk/Fpwm */
    /* 20kHz, 50000000 / 20000 =  */
    FTM0_MOD = 2500;    // 20kHz
    FTM0_CNTIN = 0x00;  // Counter Initial value
   
    /* 1 Enhanced PWM synchronization is selected. */
    FTM0_SYNCONF |= FTM_SYNCONF_SYNCMODE_MASK;
   
    /* CTNMAX = 1 - PWM update at counter in max. value */
    FTM0_SYNC |= FTM_SYNC_CNTMAX_MASK;

    /* Disable all channels outputs using the OUTPUT MASK feature.*/
    DISABLE_PWM_OUTPUT();

    FTM0_COMBINE = FTM_COMBINE_SYNCEN0_MASK | FTM_COMBINE_COMBINE0_MASK ;
   
    /* polarity setting, 3ppa driver high sides are active low */
    FTM0_POL = FTM_POL_POL1_MASK;
   
    /* Initial setting of value registers */
    FTM0_C1V = 0;
   
    /* SWSYNC = 1 - set PWM value update. This bit is cleared automatically */
    FTM0_SYNC |= FTM_SYNC_SWSYNC_MASK;

    /* Main loop */
    /* ELSnB:ELSnA = 1:0 Set channel mode to generate positive PWM */
    FTM0_C1SC |= FTM_CnSC_ELSB_MASK ;

    FTM0_MODE |= FTM_MODE_INIT_MASK;
   
    /* Set system clock as source for FTM0 (CLKS[1:0] = 01) */
    FTM0_SC |= FTM_SC_CLKS(1);  // System clock

<background>

DutyCycle = 1250;

FTM0_C1V = DutyCycle;   // 825(PWM 33%) => 0.9V => 3A

FTM0_PWMLOAD = FTM_PWMLOAD_LDOK_MASK;           // LDOK (set value)

2 Replies

1,515 Views
franksdyang
Contributor I

I cleared the problem.

it was other problem.

1,515 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Frank,

Thank you very much for your focus on Freescale Kinetis product. I am glad to provide service for you.

It sould like you had already solved your question from your second state, so please inform me to confirm that.

I'm looking forward to your reply.

Best regards,

Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply