FTM for variable pulse widths

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTM for variable pulse widths

1,821件の閲覧回数
JBM
Contributor V

I am trying to get the FTM module to allow me to create a chain of pulses on a GPIO with varying widths -- all with 50% duty cycle and then turn the FTM module off at the end of the train of pulses.  I thought I could change the MOD and CnV values in the interrupt, but it doesn't seem to work.  Here is the FTM configuration:

ftm_data.data = 0xAAAA;
ftm_data.mask = 0x8000;

// Turn on
SIM_SCGC3 |= SIM_SCGC3_FTM3_MASK;
PORTD_PCR3 = PORT_PCR_MUX(GPIO_PCR_MUX_ALT4) | PORT_PCR_DSE_MASK;

FTM3_MODE |= FTM_MODE_WPDIS_MASK;
FTM3_SC = 0x0;
FTM3_CONF = 0x0;
FTM3_CNT = 0x0;
FTM3_C3SC = FTM_CnSC_MSA(0x1) | FTM_CnSC_ELSA(1) | FTM_CnSC_ELSB(0);
FTM3_MOD = FTM_PERIOD_START;
FTM3_C3V = FTM3_MOD/2;
FTM3_SC = FTM_SC_CLKS(0x1) | FTM_SC_PS(0x0) | FTM_SC_TOIE_MASK;

enable_irq(FTM3_IRQn);

Here is the interrupt:

void FTM3_IRQHandler(void)
{
   if (FTM3_SC & FTM_SC_TOF_MASK)
   {
      FTM3_SC &= ~FTM_SC_TOF_MASK;
      if (ftm_data.mask)
      {
         FTM3_MOD = ftm_data.data & ftm_data.mask ? FTM_PERIOD_LOGICAL_ZERO : FTM_PERIOD_LOGICAL_ONE;
         FTM3_C3V = FTM3_MOD/2;
         FTM3_PWMLOAD |= FTM_PWMLOAD_LDOK_MASK;

         ftm_data.mask >>= 1;
      }
      else
      {
         FTM3_SC = 0x0;
      }
   }
}

The idea was to have an initial pulse period defined by FTM_PERIOD_START in the first code snippet.  Then in the interrupt set a long or short pulse depending on the data set in ftm_data.data and'd with ftm_data.mask.  The pulse widths I need are anywhere from 6 us to 40 us.  

ftm_data is a global structure with two members, data and mask.

Am I going about this the wrong way?  What I get is 9 pulses (should be 17).  Also, the duty cycle of the first pulse varies and the successive pulses all appear have either a 0 or 100% duty cycle.  Not sure what to do at this point.

I'm using the K64 Freedom Board and KDS 3.0, if it matters.

Thanks.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,714件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Have you try to update the register value in channel interrupt?

Example of the Output Compare mode when the match toggles the.png
For more detail about the register update, please refer "40.4.10 Registers updated from write buffers" of
K64P144M120SF5RM.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,714件の閲覧回数
JBM
Contributor V

I did.  I never got it to work.  I was able to do what I need to do with the PIT.  This can be closed.

0 件の賞賛
返信