Hi 相国 尹
Thanks for pointing out the RM content.
Could you tell me, why do you think it is needed to modify to : “However,it is expected that the FTM counter be synchronized only by the enhanced PWM Synchronization”.
The RM content is telling the customer that, if need to use the FTM synchronized function, they need to use the enhanced PWM synchronization mode, I think your sentence is the same meaning, maybe just some description difference.
Anyway, thanks for your contribution.
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------