FTM and timer sample code for Kinetis SDK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTM and timer sample code for Kinetis SDK

1,629件の閲覧回数
adongare
Contributor I

Are there any sample applications to use the FTM module for other functionality like interrupt generation, input capture, output compare and external clock inputs? The only demo included in Kinetis SDK v2.0 is a very limited PWM application which doesn't help much with developing other timer applications.

Is FTM the right module to use for generating accurate delays in applications. Should I be looking at another timing module for this purpose (Sleep mode and energy consumption are not my current focus)? Which Kinetis timer system is preferred for use as the core of an RTOS?

Platform: I'm using the bare bones SDK with ARM GCC embedded from launchpad on OSX

ラベル(2)
0 返答(返信)