FTM and timer sample code for Kinetis SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FTM and timer sample code for Kinetis SDK

1,643 Views
adongare
Contributor I

Are there any sample applications to use the FTM module for other functionality like interrupt generation, input capture, output compare and external clock inputs? The only demo included in Kinetis SDK v2.0 is a very limited PWM application which doesn't help much with developing other timer applications.

Is FTM the right module to use for generating accurate delays in applications. Should I be looking at another timing module for this purpose (Sleep mode and energy consumption are not my current focus)? Which Kinetis timer system is preferred for use as the core of an RTOS?

Platform: I'm using the bare bones SDK with ARM GCC embedded from launchpad on OSX

0 Replies