FTDI chip interfacing to TWRK60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FTDI chip interfacing to TWRK60

1,534 Views
lokeshbhatt
Contributor I

In our project we have a requirement of USB Host CDC support.

I was just evaluating, USB Stack 4.1.1 (bare metal) example Host CDC on TWR-K60N512 code warrior 10.6.

USB CDC device i want to interface with TWR kit is FT232R based device.

I want to confirm, how can we provide support for FT232R in USB Host CDC example. so it can communicate easily.

does anyone tried this thing?


Labels (2)
0 Kudos
Reply
1 Reply

1,342 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Lokesh Bhatt,

I think FTDI chip needs special driver to work with the CDC Host such as PC, so you have to know details about its spec, usually it is provided by the vendor, and then add support for it in CDC Host such as TWR-K60N512.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply