FTDI chip interfacing to TWRK60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FTDI chip interfacing to TWRK60

1,546件の閲覧回数
lokeshbhatt
Contributor I

In our project we have a requirement of USB Host CDC support.

I was just evaluating, USB Stack 4.1.1 (bare metal) example Host CDC on TWR-K60N512 code warrior 10.6.

USB CDC device i want to interface with TWR kit is FT232R based device.

I want to confirm, how can we provide support for FT232R in USB Host CDC example. so it can communicate easily.

does anyone tried this thing?


ラベル(2)
0 件の賞賛
返信
1 返信

1,354件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Lokesh Bhatt,

I think FTDI chip needs special driver to work with the CDC Host such as PC, so you have to know details about its spec, usually it is provided by the vendor, and then add support for it in CDC Host such as TWR-K60N512.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信