FSL_USB_STACK problems with 10.6

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FSL_USB_STACK problems with 10.6

1,107 次查看
arunkumar1989
Contributor I

Hello Everyone,

I am facing an unusual problem with the custom component created by Mr Erich Styger. Link -> FSL_USB_Stack

I am using a MK60FN1MOV with CW 10.6.

I am able to use the component normally,but when ever i close the project and re-open it again ,i get this error in the CDC component.

error.PNG.png

Its very frustrating to delete the "FSL_USB_STACK" components and again add it,whenever i open my project.

Is there a way around this?

Thanks in Advance

Arun

0 项奖励
回复
2 回复数

963 次查看
BlackNight
NXP Employee
NXP Employee

This is a known bug/issue in Processor Expert, and shortly after that MCU10.6 update came out, a workaround has been added to the FSL_USB_Stack component.

That you see this problem let me think that you are not using the latest components.

Are you using the latest version from SourceForge (McuOnEclipse - Browse /PEx Components at SourceForge.net, latest release right now is from 27-Dec-2014).

See McuOnEclipse Releases on SourceForge | MCU on Eclipse how to download/install them.

I hope this helps,

Erich

963 次查看
arunkumar1989
Contributor I

Hello Erich,

Yes that did the trick, I downloaded the latest PEx components and now the CDC component module is not giving that error.

Thank you,

Arun

0 项奖励
回复