FSL_Kinetis_bootloader with KDS or Codewarrior IDE

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FSL_Kinetis_bootloader with KDS or Codewarrior IDE

6,707 次查看
kwanghoPARK
Contributor II

I need the KBOOT example that can be used in the KDS or Codewarrior IDE.

Anyone knows How to use the FSL_Kinetis_Bootloader_1_1_0 with KDS IDE.

My target board is TWR-KL25Z48M.

标签 (2)
13 回复数

6,063 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi KWANGHO PARK,

KBOOT has not been supported by KDS yet.

KBOOT will only support IAR. We are planning to include KDS in the future.

Best Regards,

Iva

0 项奖励
回复

6,063 次查看
kwanghoPARK
Contributor II

Hello Iva,

Many thanks for your information.

Could you please let me know the month or quarter of you mentioned "in the Future".

Best Regards.

Park.

0 项奖励
回复

6,063 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi KWANGHO PARK,

You can look forward to new KBOOT 1.2 version planned for June,2015.

There would be KDS support.

Best Regards,

Iva

0 项奖励
回复

6,063 次查看
a8Chcx
Contributor V

Hi Iva,

Any update on this boot-loader?

Thanks,

Christie

0 项奖励
回复

6,063 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi KWANGHO PARK,

I sent email to product manager for exact information about the term. When I receive the information, I will write you.

You are welcome.

Have a nice day,

Iva

0 项奖励
回复

6,063 次查看
a8Chcx
Contributor V

Hi Iva,

I am looking for Kinetis Bootloader for my K64 using KDS IDE... I want CANBUS interface is added.

Could you let me know when it will be available, hopefully in Q2, 2015?

Thanks,

Christie

0 项奖励
回复

6,063 次查看
ivadorazinova
NXP Employee
NXP Employee

Dear Christie, CAN interface will be available on KV4x, which is planned in KBOOT 1.2. release in June, 2015. Best Regards, Iva

0 项奖励
回复

6,063 次查看
a8Chcx
Contributor V

Hi Iva,

This will be using KDS? And it is easy to modify to use on K64F?

Thanks,

Christie

0 项奖励
回复

6,063 次查看
ivadorazinova
NXP Employee
NXP Employee

Hi Christie,

yes. Here will be support for KDS and IAR.

Yes, it would be possible to port to FRDM-K64F.

Best Regards,

Iva

0 项奖励
回复

6,063 次查看
a8Chcx
Contributor V

Hi Iva,

Any update on this bootloader?

Thanks,

Christie

0 项奖励
回复

6,063 次查看
ivadorazinova
NXP Employee
NXP Employee

Hello Christie,

many thanks for your interest and for remainder.

The KBOOT 1.2 is now prepared and during the next week will be available.

Have a great day!

Iva

0 项奖励
回复

6,063 次查看
mjbcswitzerland
Specialist V

Hi

Note that KBOOT V1.1.0  UART and USB modes are available in the uTasker serial loader (together with composite USB-MSD, and/or combined SD card etc.) which can be built with CW, KDS, IAR, uVision, CooCox, Crossworks, Atollic, GCC (and with Green Hills in the developer version): µTasker Kinetis support

The TWR-KL25Z48M is supported out-of-the-box - I will post a binary later today so that it can be evaluated if required before Feescale's solution is made available.

The majority of Freescale KE, KL and K boards are supported and need no further porting effort but can be easily customised/built with any of these compilers/tools..

Regards

Mark

0 项奖励
回复

6,063 次查看
mjbcswitzerland
Specialist V

Hi

This is the link that I wanted to give earlier:

http://www.utasker.com/kinetis/TWR-KL25Z48M.html

Here you can test KBOOT operation on UART and USB on the TWR-KL25Z48M - at the same time is allows USB-MSD operation on its composite USB device connection.

To verify loading there is an application for the board with various functions (including):

- displays accelerometer values
- allows low power modes
- operates as composite USB-device with USB-CDC, mouse and keyboard (the command line menu is available of the virtual COM or on UART-0)

At the moment the KBOOT PC SW has a problem with USB mode and takes about 3 minutes to load the application. Using KBOOT UART is a lot faster and using USB-MSD is very fast.

Regards

Mark

http://www.utasker.com/kinetis.html