FRDMk64: 0 available SWD Devices detected

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDMk64: 0 available SWD Devices detected

Jump to solution
4,063 Views
SISKO
Contributor I

Hi,

I know this topic has been revised over and over, but still cant make it work.

Im usin mcuXpresso IDE.


Board was working fine until some code i made seem to broke it.
When trying to debug the board, it appears this message:

0 available SWD Devices detected.
Connect a device and try again.

Ive tried changing the K20  bootloader on the on the board. Tried openSDA 2.2 and also DAPLINK. None of them worked.

Also tried Mass Erase option from the GUI Flash Tool and Ressurect Locked Device. Both options returned with error.

Please find attached the console when tried the Ressurect Locked Device action.

Dap error.pngDap error.png

 

Is there anything i can make without using another board/programmer to program it? Maybe a flash erase by using some combination of jumpers?

Thanks

0 Kudos
Reply
1 Solution
4,053 Views
nxf58904
NXP Employee
NXP Employee
0 Kudos
Reply
3 Replies
4,054 Views
nxf58904
NXP Employee
NXP Employee

Did you change some pins? 

This link has similar issue , I hope it help you.

https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-Mke15z-in-MCUXpresso-IDE/td-p/1205300

0 Kudos
Reply
4,034 Views
SISKO
Contributor I

It worked!

You dont know how greatfull i am to you.

Solved by pressin the SW3 while debuggin/programmin

Big big THANK YOU!

Have a nice day!

0 Kudos
Reply
4,060 Views
SISKO
Contributor I

Tried J-LINK bootloader binary image. Loadded succesfully. When tried to connect with J-Link, it returned error Dap error2.pngDap error2.png

0 Kudos
Reply