FRDMk64: 0 available SWD Devices detected

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FRDMk64: 0 available SWD Devices detected

跳至解决方案
3,072 次查看
SISKO
Contributor I

Hi,

I know this topic has been revised over and over, but still cant make it work.

Im usin mcuXpresso IDE.


Board was working fine until some code i made seem to broke it.
When trying to debug the board, it appears this message:

0 available SWD Devices detected.
Connect a device and try again.

Ive tried changing the K20  bootloader on the on the board. Tried openSDA 2.2 and also DAPLINK. None of them worked.

Also tried Mass Erase option from the GUI Flash Tool and Ressurect Locked Device. Both options returned with error.

Please find attached the console when tried the Ressurect Locked Device action.

Dap error.png

 

Is there anything i can make without using another board/programmer to program it? Maybe a flash erase by using some combination of jumpers?

Thanks

0 项奖励
回复
1 解答
3,062 次查看
nxf58904
NXP Employee
NXP Employee
0 项奖励
回复
3 回复数
3,063 次查看
nxf58904
NXP Employee
NXP Employee

Did you change some pins? 

This link has similar issue , I hope it help you.

https://community.nxp.com/t5/Kinetis-Microcontrollers/FRDM-Mke15z-in-MCUXpresso-IDE/td-p/1205300

0 项奖励
回复
3,043 次查看
SISKO
Contributor I

It worked!

You dont know how greatfull i am to you.

Solved by pressin the SW3 while debuggin/programmin

Big big THANK YOU!

Have a nice day!

0 项奖励
回复
3,069 次查看
SISKO
Contributor I

Tried J-LINK bootloader binary image. Loadded succesfully. When tried to connect with J-Link, it returned error Dap error2.png

标记 (1)
0 项奖励
回复