FRDM-Mke15z in MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-Mke15z in MCUXpresso IDE

ソリューションへジャンプ
12,718件の閲覧回数
Shaanu
Contributor I

I am new to MCUXpresso IDE, I am working on frdm-mke15z, Intially my debugger was working but when I tried to configure some pin in input configuration I got below error.

Executing flash operation 'Resurrect locked Kinetis device' (Resurrect locked Kinetis device) - Wed Dec 30 21:07:47 IST 2020
Checking MCU info...
Scanning for targets...
Executing flash action...
MCUXpresso IDE RedlinkMulti Driver v11.2 (Sep 22 2020 13:23:35 - crt_emu_cm_redlink.exe build 19)
( 0) Reading remote configuration
Wc(03). No cache support.
Found chip XML file in C:/Electrolux/frdmke15z_gpio_led_output/Debug\MKE15Z256xxx7.xml
( 5) Remote configuration complete
Reconnected to existing LinkServer process.
Connecting to probe 1 core 0 (using server started externally) reports:
'Ee(42). Could not connect to core.'
Retrying...
Reconnected to existing LinkServer process.
Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.
============= SCRIPT: kinetismasserase.scp =============
Kinetis Mass Erase Script
Error: Wire Ack Fault - target connected?
Assert NRESET
Reset pin state: 00
Error: Wire not connected
Power up Debug
Error: Wire not connected
Error: Wire not connected
No Debug Power
============= END SCRIPT ===============================
Failed on connect: Ee(42). Could not connect to core.
No connection to chip's debug port
(100) Target Connection Failed
Unable to perform operation!
Command failed with exit code 1

After that not able to debug any code. After going through many posts, I encoutered that it seems to be locked kinetis. 

  Please I need help on this ,how to unlock kinetis as I m using usb cable to PC .

 

タグ(1)
0 件の賞賛
返信
1 解決策
12,659件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

 

I have recur the issue. And this issue can be caused by SWD pins' wrong configuration.

 

1.png

And I have fixed it. The step as follows.

1st.Plug out the board.

2st.Press NMI button

3st.Plug in.

4st. Download a normal code.

I hope this will help you.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

 

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
12,660件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

 

I have recur the issue. And this issue can be caused by SWD pins' wrong configuration.

 

1.png

And I have fixed it. The step as follows.

1st.Plug out the board.

2st.Press NMI button

3st.Plug in.

4st. Download a normal code.

I hope this will help you.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

 

0 件の賞賛
返信
12,652件の閲覧回数
Shaanu
Contributor I

Thanks, it worked!!!

0 件の賞賛
返信
12,670件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

If your opensda's firmware is not jlink, you need an external jlink.

Please have a try .

I hope this help you .

 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 件の賞賛
返信
12,669件の閲覧回数
nxf58904
NXP Employee
NXP Employee

nxf58904_6-1609904807330.pngnxf58904_7-1609904821222.png

 

 

0 件の賞賛
返信
12,665件の閲覧回数
Shaanu
Contributor I

I have used openSDA firmware jlink,I found below error, please help on it.

SEGGER J-Link Commander V6.86 (Compiled Sep 24 2020 17:33:12)
DLL version V6.86, compiled Sep 24 2020 17:31:31

Connecting to J-Link via USB...O.K.
Firmware: J-Link OpenSDA 2 compiled May 27 2019 11:01:03
Hardware version: V1.00
S/N: 621000000
VTref=3.300V


Type "connect" to establish a target connection, '?' for help
J-Link>connect
Please specify device / core. <Default>: MKE15Z256XXX7
Type '?' for selection dialog
Device>
Please specify target interface:
J) JTAG (Default)
S) SWD
T) cJTAG
TIF>s
Specify target interface speed [kHz]. <Default>: 4000 kHz
Speed>
Device "MKE15Z256XXX7" selected.


Connecting to target via SWD
InitTarget() start
InitTarget()
Connect Under Reset
Communication error while accessing MDM-AP.
Connect Under Reset
InitTarget() end
InitTarget() start
InitTarget()
Connect Under Reset
Communication error while accessing MDM-AP.
Connect Under Reset
InitTarget() end
InitTarget() start
InitTarget()
Connect Under Reset
Communication error while accessing MDM-AP.
Connect Under Reset
InitTarget() end
InitTarget() start
InitTarget()
Connect Under Reset
Communication error while accessing MDM-AP.
Connect Under Reset
InitTarget() end
Cannot connect to target.
J-Link>

 

0 件の賞賛
返信
12,668件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

The way to unlock kinetis via GUI as follow shows

nxf58904_0-1609904492521.png

And the way to unlock kinetis via jlink command as follow shows

 

 

 

 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信
12,682件の閲覧回数
nxf58904
NXP Employee
NXP Employee

Hi,

Can I ask which pin you set ?

Do you have a try to unlock kinetis by GUI flash tool in MCUXpresso,or use a jlink to unlock kinetis

 

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信
12,679件の閲覧回数
Shaanu
Contributor I

Thanks for reply.

 I have set PE16, pin number 1.I tried GUI flash tool but it does not unlock kineties,

I don't have idea how to connect j-link externally(any soldering is required on board?).Please guide me for j-link.

0 件の賞賛
返信