FRDM-KW41Z

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,957件の閲覧回数
surender1896
Contributor I

How to read multiple ADC channel values on FRDM-KW41Z, can anyone post the example or code for it

ラベル(1)
0 件の賞賛
返信
1 解決策
1,854件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Sureneder, I hope you’re doing well!

 

The ADC examples are included in the SDK that you can download from our online SDK builder.

When the SDK is downloaded and installed, you can access the examples from the Quickstart panel in MCUXpresso, by clicking on the "Import SDK example(s)…".

On the screen that opens, you can select your board, and then you'll find a list with all the examples for the board you chose, and there you will find our ADC examples, as well as other useful examples.

 

I hope this helps you.

 

Best regards,

Sebastian

元の投稿で解決策を見る

2 返答(返信)
1,855件の閲覧回数
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hello Sureneder, I hope you’re doing well!

 

The ADC examples are included in the SDK that you can download from our online SDK builder.

When the SDK is downloaded and installed, you can access the examples from the Quickstart panel in MCUXpresso, by clicking on the "Import SDK example(s)…".

On the screen that opens, you can select your board, and then you'll find a list with all the examples for the board you chose, and there you will find our ADC examples, as well as other useful examples.

 

I hope this helps you.

 

Best regards,

Sebastian

1,854件の閲覧回数
surender1896
Contributor I

Thank you sebastian

0 件の賞賛
返信