FRDM KW40 linker error in iar workbench

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM KW40 linker error in iar workbench

2,905件の閲覧回数
shailavsurve
Contributor II

hello there ,

i imported KW40 project in iar workbench.i am facing iar workbench error as below.iar error.png

can anyone help me??

ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,731件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi ,

IAR Undefined external messages for inline functions has explained the compiled error, please refer to it for details.

I was wondering if you can upload the project, then I can replicate the issue on my site and it can help me to figure out the root cause of the issue.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,731件の閲覧回数
shailavsurve
Contributor II

ok thanks for your support. i am uploading project here:https://www.dropbox.com/s/0kcrb0mf80fcfe6/bluetooth_heart_rate_sensor.rar?dl=0

can you download this project??

0 件の賞賛
返信

2,731件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Shailav Surve,

After double checks, I think the uploaded project had already been modified.

So I was wondering if you can share the path that the project resides in, then I can open the project on site and I've already built several demos, they don't have any error messages after built.
Have a great day,
Ping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,731件の閲覧回数
egoodii
Senior Contributor III

Is your outermost layer procedure named 'main', per C standard?

0 件の賞賛
返信

2,731件の閲覧回数
shailavsurve
Contributor II
0 件の賞賛
返信