FRDM-KW38 Configuring pin voltage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KW38 Configuring pin voltage

ソリューションへジャンプ
1,811件の閲覧回数
Dharani_Palanisamy
Contributor I

Hello Everyone,

I have started working with #FRDM-KW38. I use another board X for ECG Data acquisition. I need to connect Board X and FRDM-KW38 through @SPI and also supply board X a 5V and 3.3V from FRDM-KW38. 

My questions now, 

1. I am thinking of using 5V source from J3 pin#5 and 3.3V from J3 pin#4. Is this correct or possible?

2. How to configure J3 pin#4 from 1.8V to 3.3V ?

Disclaimer : I am a student and a newbee to this world of NXP. 
Thank you,
Dharani. 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,794件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @Dharani_Palanisamy

Hope you are doing well.

You should be able to get 5V from J3-5 as this pin should be connected to USB Host 5V.

To achieve 3V on J3-4, you would need to make some hardware modifications to your board, this may involve changing DCDC configuration (Power configuration) from Buck mode (default) to Bypass mode. For more information on this, please refer to the FRDM-KW38 Schematics included in the Hardware design files that can be downloaded from the FRDM-KW38 webpage, Design Resources section:

EduardoZamora_0-1700169949099.png

Regards,
Eduardo.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,795件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @Dharani_Palanisamy

Hope you are doing well.

You should be able to get 5V from J3-5 as this pin should be connected to USB Host 5V.

To achieve 3V on J3-4, you would need to make some hardware modifications to your board, this may involve changing DCDC configuration (Power configuration) from Buck mode (default) to Bypass mode. For more information on this, please refer to the FRDM-KW38 Schematics included in the Hardware design files that can be downloaded from the FRDM-KW38 webpage, Design Resources section:

EduardoZamora_0-1700169949099.png

Regards,
Eduardo.

0 件の賞賛
返信