FRDM-KL82Z no tty interface anymore

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL82Z no tty interface anymore

ソリューションへジャンプ
28,668件の閲覧回数
michshell
Contributor II

Hello all,

I directly copied and pasted the bin file to the board at that time still can be recongnized as a tty interface.  However, after status led flashed quickly and I unplugged and plugged the cable again, the tty interface has gone.  Also if now I use the Xpresso IDE to flash some other axf to the board.  It would show probe cannot be found.

Anyone knows how to get the usb driver back?  Thanks a lot. 

Screen Shot 2020-10-11 at 2.11.27 AM.pngScreen Shot 2020-10-11 at 2.11.27 AM.png

But it still appears as the bootloader driver,

Screen Shot 2020-10-11 at 2.16.02 AM.pngScreen Shot 2020-10-11 at 2.16.02 AM.png

 

 

0 件の賞賛
返信
1 解決策
28,513件の閲覧回数
nxf56274
NXP Employee
NXP Employee

Do you try swd?

2.PNG2.PNG

元の投稿で解決策を見る

0 件の賞賛
返信
23 返答(返信)
1,109件の閲覧回数
michshell
Contributor II

I purchased a new jlink mini edu from segger and then attached it to J19 of the board (FRDM-KL82Z) and I tried it on SWG interface.  All the problems are gone.

Thank you!

0 件の賞賛
返信
1,101件の閲覧回数
nxf56274
NXP Employee
NXP Employee

nice

タグ(1)
0 件の賞賛
返信
1,121件の閲覧回数
michshell
Contributor II

Right, I tried it on J19.  The error output about connection is slightly different, something like 'encouter error while accessing to MDM-AP'.  And if I continue with 'unlock kinetis', it gives the same error message as I previously posted.

0 件の賞賛
返信