FRDM-KL82Z no tty interface anymore

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KL82Z no tty interface anymore

Jump to solution
28,749 Views
michshell
Contributor II

Hello all,

I directly copied and pasted the bin file to the board at that time still can be recongnized as a tty interface.  However, after status led flashed quickly and I unplugged and plugged the cable again, the tty interface has gone.  Also if now I use the Xpresso IDE to flash some other axf to the board.  It would show probe cannot be found.

Anyone knows how to get the usb driver back?  Thanks a lot. 

Screen Shot 2020-10-11 at 2.11.27 AM.pngScreen Shot 2020-10-11 at 2.11.27 AM.png

But it still appears as the bootloader driver,

Screen Shot 2020-10-11 at 2.16.02 AM.pngScreen Shot 2020-10-11 at 2.16.02 AM.png

 

 

0 Kudos
Reply
1 Solution
28,594 Views
nxf56274
NXP Employee
NXP Employee

Do you try swd?

2.PNG2.PNG

View solution in original post

0 Kudos
Reply
23 Replies
1,116 Views
michshell
Contributor II

I purchased a new jlink mini edu from segger and then attached it to J19 of the board (FRDM-KL82Z) and I tried it on SWG interface.  All the problems are gone.

Thank you!

0 Kudos
Reply
1,108 Views
nxf56274
NXP Employee
NXP Employee

nice

Tags (1)
0 Kudos
Reply
1,128 Views
michshell
Contributor II

Right, I tried it on J19.  The error output about connection is slightly different, something like 'encouter error while accessing to MDM-AP'.  And if I continue with 'unlock kinetis', it gives the same error message as I previously posted.

0 Kudos
Reply