FRDM-KL28Z Keil uVision

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL28Z Keil uVision

2,489件の閲覧回数
mjk29
Contributor I

Greetings, 

I am attempting to develop a project on a FRDM-KL28Z board using Keil uVision. 

I am running into difficulties connecting to the board. 

When I attempt to setup the connection to my board in uVision I see the following. 

The board is connected through its open SDA USB port. 

I am able to see the connected volume through windows explorer. 

I can connect to the board using PUTTY. 

I can connect to the board using MCUXpresso. 

What must I do to connect using uVision?

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,344件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Matthew Kehoe,

Which version of Keil uVision are you running? I tried with the newest version 5.26.2 and I didn't face any kind of problems.

Be sure that you have the corresponding packets installed.

pastedImage_7.png

Select the debug interface that you want to use depending on the firmware that you have on the OpenSDA of your FRDM, in my case is J-Link.

pastedImage_9.png

Once you select the corresponding interface click on the setting button and you should see something like the following.

pastedImage_10.png

Please let me know the results on your side!

Hope it helps!

Victor.

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,344件の閲覧回数
mjk29
Contributor I

Thanks for the reply Victor, and sorry for the delayed response. 

I've checked that the correct pack is installed, I see the same as your picture. 

But I do not see the connected board. 

Its plugged in through the SDA port and the light is on. 

I'm using firmware from SEGGER

The J-Link OpenSDA Board specific firmware, FRDM-KL28Z.

Can you link to link to the firmware you're using?

packinstaller.png

jlink.png

0 件の賞賛
返信