FRDM-KL26Z trace on uVision with ULINK Pro Debugger

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KL26Z trace on uVision with ULINK Pro Debugger

ソリューションへジャンプ
2,816件の閲覧回数
matthieutardivo
Contributor II

Hi, I am using a FRDM-KL26Z board with a Keil ULINK Pro Debugger and I would like to trace as many information as possible on Keil uVision Debugger. Is there a way to do so ? ETM would be nice. I have seen it is possible on the KL25 version of the board but could not make it work on the KL26 board. Does anyone know how to do so ?

ラベル(2)
0 件の賞賛
返信
1 解決策
2,387件の閲覧回数
matthieutardivo
Contributor II

Final answer : It is not possible to get these debug information on uVision because MTB cannot do timestamps.

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,387件の閲覧回数
mjbcswitzerland
Specialist V

Matthieu

>>I have seen it is possible on the KL25 version of the board

Where have you seen this?

Since the KL25/KL26 have SWD and no trace pins they are limited to the CoreSight Micro Trace Buffer to provide trace capabilities.

I wouldn't envisage any differences between boards since only the SWD wires are involved. Also I wouldn't expect any debugger types to have advantages in this respect since all trace suppport would be via SWD and the controlling software.

Regards

Mark

2,387件の閲覧回数
matthieutardivo
Contributor II

Hi,

Indeed, I have made the Micro Trace Buffer work and can know trace instructions. However, I can't get any information on the event viewer, or the code coverage, or the performance analyzer.

Is it possible to get these information on uVision by using the MTB ?

Matthieu

0 件の賞賛
返信
2,387件の閲覧回数
mjbcswitzerland
Specialist V

Hi

Since the question is relevant to uVision it may be best to ask Keil directly.

Regards

Mark

0 件の賞賛
返信
2,387件の閲覧回数
matthieutardivo
Contributor II

Already done in parralel of this thread. Will provide the answer here if relevant.

0 件の賞賛
返信
2,388件の閲覧回数
matthieutardivo
Contributor II

Final answer : It is not possible to get these debug information on uVision because MTB cannot do timestamps.

0 件の賞賛
返信