FRDM-KL26Z trace on uVision with ULINK Pro Debugger

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FRDM-KL26Z trace on uVision with ULINK Pro Debugger

跳至解决方案
4,290 次查看
matthieutardivo
Contributor II

Hi, I am using a FRDM-KL26Z board with a Keil ULINK Pro Debugger and I would like to trace as many information as possible on Keil uVision Debugger. Is there a way to do so ? ETM would be nice. I have seen it is possible on the KL25 version of the board but could not make it work on the KL26 board. Does anyone know how to do so ?

0 项奖励
回复
1 解答
3,861 次查看
matthieutardivo
Contributor II

Final answer : It is not possible to get these debug information on uVision because MTB cannot do timestamps.

在原帖中查看解决方案

0 项奖励
回复
5 回复数
3,861 次查看
mjbcswitzerland
Specialist V

Matthieu

>>I have seen it is possible on the KL25 version of the board

Where have you seen this?

Since the KL25/KL26 have SWD and no trace pins they are limited to the CoreSight Micro Trace Buffer to provide trace capabilities.

I wouldn't envisage any differences between boards since only the SWD wires are involved. Also I wouldn't expect any debugger types to have advantages in this respect since all trace suppport would be via SWD and the controlling software.

Regards

Mark

3,861 次查看
matthieutardivo
Contributor II

Hi,

Indeed, I have made the Micro Trace Buffer work and can know trace instructions. However, I can't get any information on the event viewer, or the code coverage, or the performance analyzer.

Is it possible to get these information on uVision by using the MTB ?

Matthieu

0 项奖励
回复
3,861 次查看
mjbcswitzerland
Specialist V

Hi

Since the question is relevant to uVision it may be best to ask Keil directly.

Regards

Mark

0 项奖励
回复
3,861 次查看
matthieutardivo
Contributor II

Already done in parralel of this thread. Will provide the answer here if relevant.

0 项奖励
回复
3,862 次查看
matthieutardivo
Contributor II

Final answer : It is not possible to get these debug information on uVision because MTB cannot do timestamps.

0 项奖励
回复