FRDM-KEAZ128Q80 - CMSIS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KEAZ128Q80 - CMSIS

2,062 Views
mara9320
Contributor I

Is it possible to use the FRDM-KEAZ128Q80 development board with the CMSIS-DAP debugger in Keil uVision5? My development board came with PEmicro debug firmware, but I would like to switch it to CMSIS if possible. On this page: https://www.nxp.com/design/design-center/development-boards-and-designs/OPENSDA?tid=vanOpenSDA, I cannot find my device among the listed ones. I know the procedure to update the firmware, but I cannot find the file that I need to copy to the bootloader.

 

Thanks!

 

FRDM-KEAZ128 

0 Kudos
Reply
3 Replies

2,015 Views
mara9320
Contributor I

First of all thanks for your reply @Pablo_Ramos 

I downloaded CMSIS-DAP for the TRK KEA128 and there are 3 .bin files (k20dx_bl.bin, k20dx_twrkm35z75m_if_crc.bin, k20dx_twrkm35z75m_if_crc_combined.bin). I tried put them all on bootloader (also tried put them separately) but nothing happend. When I turn on my dev board after putting files in bootloader SDA_INFO is same like before:
Board Name is: FRDMP-KEAZ128Q80
MicroBoot Kernel Version is: 1.06
Bootloader Version is: 1.12
Installed Application: PEMicro FRDMP-KEAZ128Q80 Mass Storage/Debug App
Application Version is: 1.17

Can you help me figure what I am doing wrong?

Thanks!

0 Kudos
Reply

1,831 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hello, 

 

Would you please help me check the following post? 

 

FRDM-KEAZ128Q8 | OpenSDA problem - NXP Community

 

I apologize for the delay. 

 

Regards, 

Pablo 

0 Kudos
Reply

2,039 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @mara9320,

You can use the CMSIS-DAP of the TRK-KEA128 on the FRDM-KEAZ128, since both boards use the SKEAZ128MLK4 microcontroller and the debugger is compatible.

Best Regards,
Pablo

0 Kudos
Reply