FRDM-KE06Z UART0 code is not working

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-KE06Z UART0 code is not working

ソリューションへジャンプ
2,789件の閲覧回数
lajithacs
Contributor II

Kindly help me in testing UART0 of FRDM-KE06Z in transmitting a character. When the code is run no signal is coming out of UART0 transmit pin. code is attached. 

main.c

int main(void)
/*lint -restore Enable MISRA rule (6.3) checking. */
{
/* Write your local variable definition here */
uint8_t data;
uint8_t tx_array[]={0x06,0x02,0x03,0x04,0x05};
/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
PE_low_level_init();
/*** End of Processor Expert internal initialization. ***/
/* Initialization of SS1 component */
// Error = SS1_ReceiveBlock(MySPIPtr, InpData, BLOCK_SIZE); /* Request data block reception */

UART0_Init();
//SPI0_mstrInit();
for(;;)
{

UART_tx(0x55);

}

uart.c

void UART0_Init()
{

SIM_PINSEL0 |= SIM_PINSEL_UART0PS_MASK; //uart0 pin select
SIM_SCGC |= SIM_SCGC_UART0_MASK ; //Bus clock to the UART0 module is enabled
UART0_BDH =0x00;
UART0_BDL =0x4E; //Baud rate reg. value SBR[12:0]=0x004E 
//UART0_C1 =UART_C1_LOOPS_MASK|UART_C1_RSRC_MASK ; // Loop back enabled and single wire uart mode

UART0_C2 |=UART_C2_TE_MASK ; //Tx enabled

}

void UART_tx(uint8_t value)

{


// while (!(UART0_S1 & UART_S1_TDRE_MASK));
while ((UART0_S1 & UART_S1_TDRE_MASK) == 0);// wait if tx buf is full

UART0_D = value;

}

0 件の賞賛
返信
1 解決策
2,511件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Lajitha CS,

   Thank you for your root problem sharing.

   If your problem is solved, please mark the correct answer to close this question, thank you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,511件の閲覧回数
mjbcswitzerland
Specialist V

Hi

I don't see an error with the UART code.

As reference I have attached three firmware versions for the FRDM-KE06Z which you can load as reference to check the HW.

uTaskerV1.4.12_FRDM-KE06Z_UART1-115kB.bin - this uses the OpenSDA VCOM UART (PTC7 for Tx and PTC6 for Rx) connection to deliver a command line menu shell. After a reset there will be a message sent at 115200 Baud and later it will respond to inputs

uTaskerV1.4.12_FRDM-KE06Z_UART0-PTB-115kB.bin - same but using UART0 (instead of UART1) and the pins are multiplexed to PTB1 for Tx and PTB0 for Rx

uTaskerV1.4.12_FRDM-KE06Z_UART0-PTA-115kB.bin - same but using UART0 (instead of UART1) and the pins are multiplexed to PTA3 for Tx and PTA2 for Rx

I build these with the uTasker project using the defines

#define FRDM_KE06Z
#define DEMO_UART    1

,

#define FRDM_KE06Z
#define DEMO_UART    0

#define UART0_ON_A

and

#define FRDM_KE06Z
#define DEMO_UART    0

respectively.

Beware that on the FRDM-KE06Z board the UART0 UART pins are not connected to the connectors by default since they are used by other peripheral connections. There are zero-Ohm resistors to modify this if needed, therefore measure the Tx output directly at the processor pins to be sure that it is not a measurement issue.

Regards

Mark


http://www.utasker.com/kinetis/FRDM-KE06Z.html

2,511件の閲覧回数
lajithacs
Contributor II

Thank you Mark. It was a hardware issue. UART0 tx signal i checked at the connector, which was not coming there as you have mentioned. Now its working .

0 件の賞賛
返信
2,512件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Lajitha CS,

   Thank you for your root problem sharing.

   If your problem is solved, please mark the correct answer to close this question, thank you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信