FRDM-K66F Run @180MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K66F Run @180MHz

3,039件の閲覧回数
a8Chcx
Contributor IV

Hi,

I am running RRDM-K66F MCU at 120MHz and everything is working fine.

For now, I am trying to run it at 180MHz. 

Can anybody tell me if there is any potential issue with the high speed? 

Thanks,

Christie

 

0 件の賞賛
返信
5 返答(返信)

3,022件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @a8Chcx,

There shouldn't be any issues, as the 180MHz frequency is still within the operating ranges of the MK66 MCU.

BR,
Edwin.

0 件の賞賛
返信

3,004件の閲覧回数
a8Chcx
Contributor IV

Hi Edwin,

I checked the document and says there is the restriction for flash programming and erasing for high speed. Does it means I can't do the flash programming and erasing?

 

If I want to do the flashing programming and erasing, I have to switch to slower speed?

Thanks,

Christie

0 件の賞賛
返信

2,988件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @a8Chcx,

Could you please clarify what document you are referring to? 

0 件の賞賛
返信

2,964件の閲覧回数
a8Chcx
Contributor IV

Hi Edwin,

It is on section 8.7 of "K66P144M180SF5RMV2" manal.

The flash memory on this device should not be programmed or erased while operating in
High Speed Run or VLPR power modes.

Thanks,

Christie

0 件の賞賛
返信

2,950件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @a8Chcx,

Thanks for clarifying. Yes, this is a restriction on the HSRUN (180MHz) mode. If I want to do the flashing programming and erasing, you have to switch to a lower speed.

BR,
Edwin.

0 件の賞賛
返信