FRDM-K66F Run @180MHz

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K66F Run @180MHz

2,935件の閲覧回数
a8Chcx
Contributor V

Hi,

I am running RRDM-K66F MCU at 120MHz and everything is working fine.

For now, I am trying to run it at 180MHz. 

Can anybody tell me if there is any potential issue with the high speed? 

Thanks,

Christie

 

0 件の賞賛
返信
5 返答(返信)

2,918件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @a8Chcx,

There shouldn't be any issues, as the 180MHz frequency is still within the operating ranges of the MK66 MCU.

BR,
Edwin.

0 件の賞賛
返信

2,900件の閲覧回数
a8Chcx
Contributor V

Hi Edwin,

I checked the document and says there is the restriction for flash programming and erasing for high speed. Does it means I can't do the flash programming and erasing?

 

If I want to do the flashing programming and erasing, I have to switch to slower speed?

Thanks,

Christie

0 件の賞賛
返信

2,884件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @a8Chcx,

Could you please clarify what document you are referring to? 

0 件の賞賛
返信

2,860件の閲覧回数
a8Chcx
Contributor V

Hi Edwin,

It is on section 8.7 of "K66P144M180SF5RMV2" manal.

The flash memory on this device should not be programmed or erased while operating in
High Speed Run or VLPR power modes.

Thanks,

Christie

0 件の賞賛
返信

2,846件の閲覧回数
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @a8Chcx,

Thanks for clarifying. Yes, this is a restriction on the HSRUN (180MHz) mode. If I want to do the flashing programming and erasing, you have to switch to a lower speed.

BR,
Edwin.

0 件の賞賛
返信