FRDM K64F: USB MSD with SD Card Bare Metal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM K64F: USB MSD with SD Card Bare Metal

1,442 Views
giacomopetrini
Contributor IV

Hi, I found the example in the KSDK/USB floder (dev_msd_disk_frdmk64f120m_bm) that is compiling and working as expected if I select the Ram Disk.

But if I select the SD Card there is acompile error: it can't find the sd.h file.

How can I make it working?

Thank Regards Giacomo

0 Kudos
Reply
2 Replies

1,208 Views
antonioconcio
NXP Employee
NXP Employee

Ciao Giacomo,

That function is not enabled in the actual version of SDK (1.0.0), it will be enabled in the next release 1.1 that anyway will be public on December 16th so stay tuned :smileywink:.

Cheers,

Antonio

0 Kudos
Reply

1,208 Views
giacomopetrini
Contributor IV

Ahh ok thanks, at least I have a ETA for next KSDK release.

Regards Giacomo

0 Kudos
Reply