FRDM-K64F Power Connector

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K64F Power Connector

ソリューションへジャンプ
1,609件の閲覧回数
skunky
Contributor II

Does anyone know the part number of the power connector that fits on the FRDM-K64F board? The part number isn't given in the schematic since the part isn't populated. Its designator is J24.

ラベル(1)
0 件の賞賛
返信
1 解決策
1,477件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Mark:

According to the BOM (Bill of Materials), the part number that would fit in there is PJ1-022.

For reference and to check any other component, you can download the BOM and design files from the next link, under "Printed Circuits Boards and Schematics":

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-K64F&fpsp=1&tab=Design_Tools_Tab


Regards!,
Jorge Gonzalez


-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,478件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Mark:

According to the BOM (Bill of Materials), the part number that would fit in there is PJ1-022.

For reference and to check any other component, you can download the BOM and design files from the next link, under "Printed Circuits Boards and Schematics":

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=FRDM-K64F&fpsp=1&tab=Design_Tools_Tab


Regards!,
Jorge Gonzalez


-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信