FRDM-K64F Debug

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-K64F Debug

1,588 次查看
LArmstrong1985
Contributor III

Hi, I bought a new FRDM-K64F board, but I've same problems with OpenSDAv2 Debug.

The default bootloader installed is MBED but it has several connection problems and often crashes

whit the following error:

"crt_emu_cm_redlink has stopped working mcuxpresso "

I tried to replace it with Segger Jlinker OpenSDA Firmware, that I think is better, but when I put the
bin in the virtual folder it return this error in the log (fails.txt):
RESERVED BITS
How I can resolve this problems and works properly with this board?
Thank you very much!
0 项奖励
回复
1 回复

1,280 次查看
mjbcswitzerland
Specialist V

Hi

Continue using the Segger OpenSDA since it is basically good.

Probably the error is because you are loading code with Flash configuration values (in 0x400..0x40f range) which have values that it doesn't like. For example, the values may cause the chips to disable its debug interface and become secured, which the loader will try to protect against.

Try loading some binary file from here
http://www.utasker.com/kinetis/FRDM-K64F.html
because these will have good values and so identify whether it is due to the *.bin that you are trying to load or not.

Regards

Mark

0 项奖励
回复