FRDM-K64F Context switching MSP & PSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K64F Context switching MSP & PSP

Jump to solution
4,226 Views
luisgarabo
Contributor II

Hi,

Do you have an example of FRDM-K64F Context switching MSP & PSP?

Thanks for your help,

Labels (1)
0 Kudos
Reply
1 Solution
3,407 Views
CCandido
Contributor V

Hi Luis,

I tested it code not run, you can test.

stm32f4 - scheduler and stack - Electrical Engineering Stack Exchange 

thanks,

Carlos.

View solution in original post

0 Kudos
Reply
4 Replies
3,408 Views
miduo
NXP Employee
NXP Employee

Hi,

Please make reference the MQX RTCS code, where in boot.s, the active stack pointer is set to PSP (set bit 1 of the CONTROL register). Then no need  do any manipulation of this bit. Cortex m4 itself automatically switches the active stack pointer to MSP in handler mode and switches back to PSP with exception return.

Here is the stack pointer switch code at <boot.s>

   /* Prepare process stack pointer */
   mrs r0, MSP
   msr PSP, r0

 

   /* Switch to proccess stack (PSP) */
   mrs r0, CONTROL
   orr r0, r0, #2
   msr CONTROL, r0
   isb #15
3,408 Views
CCandido
Contributor V

Hi Luis,

I tested it code not run, you can test.

stm32f4 - scheduler and stack - Electrical Engineering Stack Exchange 

thanks,

Carlos.

0 Kudos
Reply
3,407 Views
luisgarabo
Contributor II

Thank you Carlos, Fang and Mark,

Your suggestions helped a lot. I implemented the code suggested by Carlos and I found that the priority for the PendSV call is set differently for the K64. I used the following:

NVIC_SetPriority(PendSV_IRQn, 0xF); //   Set PendSV to lowest possible priority

It works great!

Thanks!

Luis

0 Kudos
Reply
3,407 Views
mjbcswitzerland
Specialist V

Hi

You can study the FreeRTOS file /source/portable/GCC/ARM_MC4F/port.c to get some examples of such context switching.

Regards

Mark


uTasker developer and supporter (+5'000 hours experience on +60 Kinetis derivatives in +80 product developments)
Kinetis: http://www.utasker.com/kinetis.html