FRDM-K22F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K22F

1,519件の閲覧回数
josemartinez
Contributor III

Hello all,

I have just bought a FRDM-K22F, I am using the openSDA connector to debug my code, when I download my application to debug it, I can see the D2 LED flashing but at the same time the RGB led is switch on in GREEN without running the code, then I can´t switching off in anyway.

Someone can advise me why that it could be possible.

Thanks in advance.

0 件の賞賛
返信
1 返信

1,409件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Jose,

Please download the SDK_2.2_FRDM-K22F package refer Generating a downloadable MCUXpresso SDK v.2 package.

Then you can modify the led_output example to toggle the Green LED.

led_output.png

led_output SDK_2.2_FRDM-K22F.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信