FRDM-K22F, UART Rx (callback) Makes MQX Weird

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K22F, UART Rx (callback) Makes MQX Weird

ソリューションへジャンプ
2,015件の閲覧回数
jeffreygraves
Contributor III

If I send enough characters to the UART, I can make MQX act weird*.

 

*MQX will stop running a task or...

*MQX will stop running more than one task or...

*MQX will run a task open loop, ignoring wait functions (ie OSA_TimeDelay()).

 

I have attached a "bare bones" project that reproduces this behavior.

 

This project uses a UART Rx data callback function.

(This simple project does not do anything with the received chars.)

 

This project targets the FRDM-K22F development board.

 

This project uses the following software:

KDS 2.0

KSDK 1.1.0

MQX-KSDK

PEx

 

The project configuration is straight forward and what you get with PEx.

 

I have not taken any steps to install other interrupt handlers.

 

Steps to reproduce:

 

Comm settings: 115Kbps,N,8,1

Monitor the referenced I/O pins...

Repeatedly paste a string (~80 char) into a terminal app like Tera Term.

Eventually, the toggling I/O (square wave) will change indicating a MQX problem.

I have reproduced this problem with and without a Tera Term character delay (1ms).

 

Has anyone else seen this problem?

 

This issue is affecting the stability of a more complicated product.

Any feedback would be greatly appreciated.

 

Thanks,

Original Attachment has been moved to: UART_Rx_Makes_MQX_Wierd01.zip

ラベル(2)
タグ(2)
0 件の賞賛
返信
1 解決策
1,743件の閲覧回数
jeffreygraves
Contributor III

Mark,

I did also post it to "MQX Software Solutions".

https://community.freescale.com/thread/352874

I will note here if I get an answer there.

Thank you,

**Solved**

See post in "MQX Software Solutions".

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,743件の閲覧回数
mjbcswitzerland
Specialist V

Hi Jeffrey

You may have more success posting in the MQX and/or PE forums since this sounds like a software issue rather than a Kinetis/K22/UART problem.

MQX Software Solutions

https://community.freescale.com/community/pex

Regards

Mark

Kinetis: µTasker Kinetis support

K22: µTasker Kinetis FRDM-K22F support / µTasker Kinetis TWR-K22F120M support

For the complete "out-of-the-box" Kinetis experience and faster time to market

0 件の賞賛
返信
1,744件の閲覧回数
jeffreygraves
Contributor III

Mark,

I did also post it to "MQX Software Solutions".

https://community.freescale.com/thread/352874

I will note here if I get an answer there.

Thank you,

**Solved**

See post in "MQX Software Solutions".

0 件の賞賛
返信