FRDM-K22 RTC wakeup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-K22 RTC wakeup

2,426 次查看
nesrinemhiri
Contributor III

I want to configure my FRDM-K22F to wakeup from VLLS2 mode each 1second  using RTCn can someone help to configure this.

I download the SDK library but I didn't find such example 

Thanks for help 

标签 (1)
4 回复数

2,163 次查看
nesrinemhiri
Contributor III

Hello,

Thank you for your help :smileyhappy:

where can i find the code of this function :         fnSetLowPowerMode(VLLS2_MODE);

I check the example power switch mode but it is very complicated, i need a simpler code on how to enter VLLS2 mode and wake up from this mode each 1s using RTC .

Nesrine

0 项奖励
回复

2,163 次查看
mjbcswitzerland
Specialist V


Hi

As mentioned, you can get a complete solution from the uTasker project on GitHub:
https://github.com/uTasker/uTasker-Kinetis

The routine fnSetLowPowerMode(VLLS2_MODE);
does (for your processor):
SMC_STOPCTRL = (SMC_STOPCTRL_VLLSM_VLLS2);
SMC_PMCTRL = (SMC_PMCTRL_RUNM_NORMAL | SMC_PMCTRL_STOPM_LLS);
SYSTEM_CONTROL_REGISTER |= SLEEPDEEP;

which prepares for the sleep mode, which is subsequently set using wfi instruction.

Regards

Mark

P.S. Note also that SMC_PMPROT has to be written to to enable the required low power mode(s) that will be used.
Since this is a write-once register it is best written during the board start-up so that all modes that may be required at any future time point are enabled.

2,163 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi nesrine mhiri

Just add to Mark's good comments, you also can also refer to the power_mode_switch demo under the KSDK installation folder.

SDK_2.2_FRDM-K22F\boards\frdmk22f\demo_apps\power_mode_switch

This demo is to show how to switch to different power modes, and how to configure a wakeup source and wakeup the MCU from low power modes.

Regards

Daniel

2,163 次查看
mjbcswitzerland
Specialist V

Hi Nesrine

I have attached a binary file for the FRDM-K22F that will set itself to the VLSS2 mode and wake up via RTC alarm interrupt after a short delay.
Note that the wake-up is via a reset so the code restarts each time.

This is the sequence seen on the VCOM interface (UART at 115200 Baud):

Hello, world... FRDM-K22F
OS Heap use = 0x0479 from 0x6000
WOKEN - restoring WAIT mode

Serial number: 00
Software version V1.4.012
Device identification: KINETIS

     Main menu
===================
1              Configure LAN interface
2              Configure serial interface
3              Go to I/O menu
4              Go to administration menu
5              Go to overview/statistics menu
6              Go to USB menu
7              Go to I2C menu

   Admin. menu
===================
up               go to main menu
show_config      Show configuration
save             Save configuration to FLASH
reject           Reset non-saved changes
restore          Restore factory settings
show_time        Display date/time
set_time         Set time hh:mm:ss
set_date         Set Date dd:mm:yyyy
show_alarm       Display alarm d/t
set_alarm        Set alarm (date)(+)[time]
del_alarm        Delete alarm
show_lp          Show low power mode and options
set_lp           [option] Set low power mode
reset            Reset device
last_rst         Reset cause
help             Display menu specific help
quit             Leave command mode

Hello - this will show you how to use a RTC alarm
to restart the processor from a low leakage mode
We'll check the RTC is running first..

1.01.1970 00:00:51

#
1.01.1970 00:00:52

#
1.01.1970 00:00:53

#Now we set an alarm to fire in 4s time..

New alarm set
1.01.1970 00:00:58

#and we command going to VLLS2 mode....

#zzzzzzzzz...(we will wake at the RTC alarm and recover via reset)


The sequence repeats over and over again - as per your requirement (although I set longer times so that it can be better monitored).


The code that I used is as follows:

extern void fnQuickTask1(TTASKTABLE *ptrTaskTable)
{
    QUEUE_HANDLE        PortIDInternal = ptrTaskTable->TaskID;           // queue ID for task input
    unsigned char       ucInputMessage[HEADER_LENGTH];                   // reserve space for receiving messages
    static int iState = 0;
    switch (iState++) {
    case 0:
        fnInitiateLogin(ES_SERIAL_LOGIN);                               // start command line interface
        fnCommandInput("4\r\n", 3, SOURCE_SERIAL);                      // move to the admin menu
        uTaskerMonoTimer(TASK_DEV_1, (DELAY_LIMIT)(1.0 * SEC), 1);
        break;
    case 1:
        fnDebugMsg("\r\nHello - this will show you how to use a RTC alarm\r\n");
        fnDebugMsg("to restart the processor from a low leakage mode\r\n");
        uTaskerMonoTimer(TASK_DEV_1, (DELAY_LIMIT)(1.0 * SEC), 1);
        break;
    case 2:
        fnDebugMsg("We'll check the RTC is running first..\r\n");
        uTaskerMonoTimer(TASK_DEV_1, (DELAY_LIMIT)(0.2 * SEC), 1);
        break;
    case 3:
    case 4:
    case 5:
        fnCommandInput("show_time\r\n", 11, SOURCE_SERIAL); // show the present time
        uTaskerMonoTimer(TASK_DEV_1, (DELAY_LIMIT)(1.1 * SEC), 1);
        break;
    case 6:
        fnDebugMsg("Now we set an alarm to fire in 4s time..\r\n");
        fnCommandInput("set_alarm +4\r\n", 14, SOURCE_SERIAL); // set a RTC alarm to fire 4s into the future
        uTaskerMonoTimer(TASK_DEV_1, (DELAY_LIMIT)(0.2 * SEC), 1);
        break;
    case 7:
        fnDebugMsg("and we command going to VLLS2 mode....");
        fnSetLowPowerMode(VLLS2_MODE);
        fnDebugMsg("zzzzzzzzz...(we will wake at the RTC alarm and recover via reset)");
        break;
    }

    while (fnRead(PortIDInternal, ucInputMessage, HEADER_LENGTH) != 0) { // read input queue to clear timer events
    }
}

I did this in the uTasker project and using a single task to demonstrate the operation flow.
In addition, I first used code to configure the RTC to run from the board's 32kHz crystal
fnStartRTC(0);                                                   // start the RTC if it isn't yet operating
and I enabled a wake-up interrupt on SW2 and also on the RTC

    INTERRUPT_SETUP interrupt_setup;                                     // interrupt configuration parameters
    interrupt_setup.int_type       = WAKEUP_INTERRUPT;                   // configure as wake-up interrupt
    interrupt_setup.int_handler    = wakeup_interrupt;
    interrupt_setup.int_priority   = PRIORITY_PORT_C_INT;                // interrupt priority level
    interrupt_setup.int_port       = PORTC;                              // the port that the interrupt input is on
    interrupt_setup.int_port_bits  = PORTC_BIT1;                         // the input connected (SW2 on FRDM-K22F)
    interrupt_setup.int_port_sense = (IRQ_FALLING_EDGE | PULLUP_ON);     // interrupt is to be falling edge sensitive
    fnConfigureInterrupt((void *)&interrupt_setup);                      // configure wake-up on port


    interrupt_setup.int_port = PORT_MODULE;                              // define a wake-up interrupt on a module
    interrupt_setup.int_port_bits = (MODULE_RTC_ALARM);                  // wake-up on RTC alarm interrupt
    fnConfigureInterrupt((void *)&interrupt_setup);                      // configure wake-up from RTC alarm


You can get the uTasker project at the links below to simply do this and many much more power-ful things without loss of development time.

Regards

Mark

Kinetis: http://www.utasker.com/kinetis.html
K22:
- http://www.utasker.com/kinetis/FRDM-K22F.html
- http://www.utasker.com/kinetis/TWR-K22F120M.html
- http://www.utasker.com/kinetis/BLAZE_K22.html