MK20DN512VLQ10 EZP_MS bit question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MK20DN512VLQ10 EZP_MS bit question

1,385件の閲覧回数
isaotakashima
Contributor IV

I would like to migrate from MK20DN512ZVLQ10 to MK20DN512VLQ10.

I refer the  AN4445 Kinetis 100 MHz Rev 1.x to Rev 2.x Migration Guide, and I have the question.

The description of EZP_MS bit of Mode Register (RCM_MR) is as below, but I cannot find out the EZP_MS in the Chapter 10 Signal Multiplexing and Signal Descriptions.

EZP_MS_B pin state
Reflects the state of the EZP_MS pin during the last Chip Reset
0 Pin deasserted (logic 1)
1 Pin asserted (logic 0)

I believe that EZP_MS_B (EZP_MS) is wrong, EZP_CS_B (EZP_CS) should be correct.

Am I correct?

Please reply as soon as possible.

Best regards,

Takashima

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,285件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Takashima,
Yes you are right. The "EZP_MS pin" in the RCM_MR register should be "EZP_CS pin". It only change the register address, not the function.
Thank you very much.
Regards
Jing

0 件の賞賛
返信