FPU setup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FPU setup

2,094 Views
ERussell
Contributor IV

I am working with a K60FN1M processor and using CW10.4. I want to make sure that I am setting up the hardware FPU correctly. I have done the following:

1 - Selected Hardware vfpv4 in the Tool Settings under project properties.

2 - Selected c9x for the Library model

3 - Included the ewl c library

4 - Explicitly enabled the FPU by setting bits 10 and 11 in SCB_CPACR

5 - Set both the ASPEN and LSPEN in SCB_FPCCR to enable the extended exception frame and the lazy stacking options

6 - Added the suffix f to all float constants.

I am using a preemptive task scheduler rather than a full RTOS.

I want to be able to use library routines such as powf(), expf(), etc. and have them only use single precision float values. Is there a specific ewl library that I should specify or certain macros that need to be defined?

Thanks,

Elizabeth

Tags (3)
0 Kudos
Reply
1 Reply

1,689 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

There is no specific ewl library, you can use the system default one.

About enable the FPU, please check code for your reference:

; Enable the floating point coprocessor

#if defined (_VFPv4_)

       MOVW r1,#60808              ; load CPACR           

       MOVT r1,#57344              ; (0xE000ED88)

       LDR r0,[r1]

       ORR.W r0,r0,#VFPEnable      ; Enable FPU

       STR r0, [r1]                ; on CP10, CP11

       MOV.W r0,#R2N_Enable

       VMSR FPSCR, r0

#endif

Wish it helps.

0 Kudos
Reply