FOC function in KV4x or KV5x

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FOC function in KV4x or KV5x

Jump to solution
2,103 Views
deega_jung
Contributor III

Hi NXP,

Could you advice me about the FOC, below is a project inform.

Application : ESC Drone 

Require spec.

Supply Voltage : 48V

Current : 60A

Motor Control Concept : PWM Speed Control and Sensorless FOC Control

 

Please let me know if your KV4x or KV5x solution supports sensorless FOC function for motor control.

If not supported, please let me know which product is a solution that supports sensorless FOC and PWM speed control with the above specifications.

Thanks,

Deega

0 Kudos
Reply
1 Solution
2,090 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Deega,

If you are interested on the KV family for your implementation, Application Note 5237 (AN5237, link below) may be of use as a starting point for your own motor control application.

https://www.nxp.com/docs/en/application-note/AN5237.pdf

I hope that this information helps.

Regards,
Gustavo

View solution in original post

0 Kudos
Reply
2 Replies
2,091 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Deega,

If you are interested on the KV family for your implementation, Application Note 5237 (AN5237, link below) may be of use as a starting point for your own motor control application.

https://www.nxp.com/docs/en/application-note/AN5237.pdf

I hope that this information helps.

Regards,
Gustavo

0 Kudos
Reply
2,078 Views
deega_jung
Contributor III

Hello Gustavo,

Thank you for your reply, there's a lot of help.

Thanks,

Deega

0 Kudos
Reply