FBLIP Clock Mode of KEA-128?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FBLIP Clock Mode of KEA-128?

705 次查看
vigneshbalaji
Senior Contributor I

Hi,

    I want to know what is the maximum bus Clock that can be run in FLL bypassed internal low power(FBLIP) Mode???

0 项奖励
回复
1 回复

622 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi VIGNESH,

In FLL bypassed internal low-power mode, the ICSOUT clock is derived from the internal reference clock and the FLL is disabled. The internal reference clock is enabled.

You can refer the "Figure 5-1. Clocking diagram" in KEA128RM.pdf.

Clocking diagram.jpg

If all these Dividers(BDIV DIV1 DIV2) divides by 1, the frequency of Bus Clock will same as IRC.

Then you can find the ICS specifications in S9KEA128P80M48SF0.pdf.

ICS specifications.jpg

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复