Ethernet for K60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,252件の閲覧回数
pietrodicastri
Senior Contributor II

Good morning

I would like to have the drivers for TCP/IP without MQX. Is there a chance to get??

Thank you

ラベル(1)
タグ(2)
1 解決策
2,861件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Pietro,

Do you mean a bare metal TCP/IP stack for K60? If so, I think you may refer to KSDK Software Development Kit for Kinetis MCUs|Freescale , it supports lwip support, and demos for bare metal and RTOS are included in this package as well. Since there is a new space for KSDK topics already, you may ask questions regarding KSDK directly in https://community.freescale.com/community/kinetis/kinetis-software-development-kit.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,862件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Pietro,

Do you mean a bare metal TCP/IP stack for K60? If so, I think you may refer to KSDK Software Development Kit for Kinetis MCUs|Freescale , it supports lwip support, and demos for bare metal and RTOS are included in this package as well. Since there is a new space for KSDK topics already, you may ask questions regarding KSDK directly in https://community.freescale.com/community/kinetis/kinetis-software-development-kit.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,861件の閲覧回数
pietrodicastri
Senior Contributor II

Hi Kan

I have downloaded the KSDK. I don t see the ehernet support.

Is there ??

Thank You

0 件の賞賛
返信
2,861件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Pietro di Castri,

You may find the ethernet demo in the foder of "C:\Freescale\KSDK_1.0.0\demos\lwip_httpserver_demo" or something like that.

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,861件の閲覧回数
pietrodicastri
Senior Contributor II

Hi Kan_Li

Thank You for the support.

I have this situation on my demos directory. What's wrong?

I have googled for \lwip_httpserver_demo and I find a reference to the work of Adam Dunkle. Is this the stack used

for the Kinetis???

Thank You

I demos.png

0 件の賞賛
返信
2,861件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Pietro di Castri,

Seems you have installed the special version for KL03Z, actually there is no ethernet module on that chip, so no demo in that SDK, you should download the following version instead.

1.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------