Error: unable to open CMSIS-DAP device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error: unable to open CMSIS-DAP device

Jump to solution
4,480 Views
mohammadgouse
Contributor I


I purchased FRDM-K82 kit and start to test it using Kinetis design studio 3.0 in windows 10. while trying to debug with the kit i am getting following error.

Open On-Chip Debugger 0.8.0-dev (2015-01-09-16:22)

Licensed under GNU GPL v2

For bug reports, read

  http://openocd.sourceforge.net/doc/doxygen/bugs.html

Info : only one transport option; autoselect 'cmsis-dap'

Error: unable to open CMSIS-DAP device

Error: unable to init CMSIS-DAP driver

Error: Error selecting 'cmsis-dap' as transport

Runtime Error: C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg:3:

in procedure 'script'

at file "embedded:startup.tcl", line 58

in procedure 'interface' called at file "C:/Freescale/KDS_v3/openocd/bin/..//scripts/kinetis.cfg", line 3

I tried this windows 8 OS also, the result is,

Error in final launch sequence

Failed to execute MI command:

-target-select remote localhost:3333

Error message from debugger back end:

localhost:3333: The system tried to join a drive to a directory on a joined drive.

Failed to execute MI command:

-target-select remote localhost:3333

Error message from debugger back end:

localhost:3333: The system tried to join a drive to a directory on a joined drive.

localhost:3333: The system tried to join a drive to a directory on a joined drive.

0 Kudos
Reply
1 Solution
3,231 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

I would recommend customer to update FRDM-K82 board OpenSDA firmware to J-Link.

Customer could find and download Segger J-Link firmware from here.

Please let us know if there still with issues after update with J-Link firmware.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,232 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

I would recommend customer to update FRDM-K82 board OpenSDA firmware to J-Link.

Customer could find and download Segger J-Link firmware from here.

Please let us know if there still with issues after update with J-Link firmware.


Wish it helps.

Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply