Error in documentation? (KE1xFP100M168SF0RM)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Error in documentation? (KE1xFP100M168SF0RM)

跳至解决方案
1,998 次查看
xxxajk
Contributor III

Document Number: KE1xFP100M168SF0RM
Rev. 2, 09/2016

page 568 says:

ROM bootloader also supports application integrity check. It performs a CRC
check over a configurable range of flash if requested via BCA option, and
asserts a pin to indicate the failure. The available CRC check failure pin
is shown as below:
And lists PTA11


Page 633 says:
If the bootloader returns kStatus_AppCrcCheckOutOfRange or
kStatus_AppCrcCheckFailed, then an external pin (PTA6) will also be
asserted, to indicate CRC check failure.

Is it

PTA11

PTA6

or BOTH?

标签 (1)
1 解答
1,718 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Andrew,

Thank you for your feedback and sorry for any inconvenience that may cause.

Checked by the owner, the PTA6 is a typo, should be PTA11.

I reported this typo to document team for fix, thanks a lot for your finding!

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

5 回复数
1,718 次查看
xxxajk
Contributor III

Thanks! There are other typos in the documentation, sometimes a word is omitted, but I can manage to understand from the context, would you like me to post those as I find them again? Better docs helps everyone.

0 项奖励
回复
1,718 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Yes,please

0 项奖励
回复
1,718 次查看
xxxajk
Contributor III

Sorry I have not had time to add a lot here, been very busy...

Here's an obvious one for you to forward to the documentation team.

Page 1199

45.4.1.2 Software reset
Writing 1 to CR[SWR] forces the equivalent of a POR to the rest of the RTC module.
CR[SWR] is not affected by the software reset and must be cleared by software. The
access control registers are not affected by either VBAT POR or the software reset; they
are reset by the chip reset.

There is no VBAT on this device. :-)

0 项奖励
回复
1,718 次查看
xxxajk
Contributor III

I'll make a collection on this and other RM/DS over the weekend.

Errors like this have stalled progress for my client's next product, but that's the way it goes sometimes.

Happy to lend a hand.

1,719 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Andrew,

Thank you for your feedback and sorry for any inconvenience that may cause.

Checked by the owner, the PTA6 is a typo, should be PTA11.

I reported this typo to document team for fix, thanks a lot for your finding!

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------