Error Erasing flash of device at the end of download.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error Erasing flash of device at the end of download.

ソリューションへジャンプ
2,922件の閲覧回数
w_lingjun
Contributor III

Hi,

I am working on S32DS and a PE Multilink tool to debug.The microcontroller is SKEAZ128.

The download and debug worked well before, but someday, when I download a project, got following error. Then I new a simple project or examples from NXP, also got the same error.

It seems that this error is not related to software.

By the way, I download LIN_stack_S12_4_6_3.exe from NXP website and intall it in the same folder with S32DS_ARM_v2.0, I don't know whether it has any effects. I also try to remove this stack and unstall S32DS, but it still have following error.

I find similar problems in this community, but there is not a clear reply to solve this problem.

Someone say it is the problem of P&E multilink, after updating the device, the problem resolved. And I update the fireware of P&E multilink, the problem still exists.

Can anyone help me?

Connection from "127.0.0.1" via 127.0.0.1
Connection from "127.0.0.1" via 127.0.0.1
PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read registers while part is running.
Telnet server running on 127.0.0.1:51794
Copyright 2012 P&E Microcomputer Systems,Inc.
Command Line :C:\NXP\S32DS_ARM_v2.0\eclipse\plugins
\com.pemicro.debug.gdbjtag.pne_3.1.1.201708081924\win32\pegdbserver_console -
device=NXP_KEx_S9KEAZ128M4 -startserver -singlesession -serverport=7224 -
gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -p?

CMD>RE

Initializing.
Target has been RESET and is active.
CMD>CM C:\NXP\S32DS_ARM_v2.0\eclipse\plugins
\com.pemicro.debug.gdbjtag.pne_3.1.1.201708081924\win32\gdi\P&E\supportFiles_ARM\NXP
\KEx\freescale_s9keaz128m4_pflash.arp

Initializing.
Initialized.

;version 1.03, 06/02/2014, Copyright 2014 P&E Microcomputer Systems, Inc. All rights
reserved. www.pemicro.com [ke_128k_pflash_ftmre_m0]

;device freescale, s9keaz128m4, pflash

;begin_cs device=$00000000, length=$00020000, ram=$20000000

Loading programming algorithm ...

WARNING - Selected .ARP file has been modified. CRC16 = $2AD1
Done.
CMD>VC
Command is inactive for this .ARP file.

CMD>EM
Command is inactive for this .ARP file.
Error Erasing flash of device
Error occured during Flash programming.

Best regards,

Sarah

ラベル(1)
0 件の賞賛
返信
1 解決策
2,875件の閲覧回数
w_lingjun
Contributor III

This is because that the SBC UJA1167 on my board is in relaease mode when I debug.

After I reset the SBC enter into forced normal mode, the download is OK.

• pin RSTN is held LOW
• CANH is pulled up to VBAT
• CANL is pulled down to GND

Above actions for 1~2s can make a SBC system reset.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,876件の閲覧回数
w_lingjun
Contributor III

This is because that the SBC UJA1167 on my board is in relaease mode when I debug.

After I reset the SBC enter into forced normal mode, the download is OK.

• pin RSTN is held LOW
• CANH is pulled up to VBAT
• CANL is pulled down to GND

Above actions for 1~2s can make a SBC system reset.

0 件の賞賛
返信
2,904件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @w_lingjun,

That's strange, the error log mention that the arp file (programming algorithm) was modified. Also, I see that you're using the S32DS 2.0 version, I will suggest updating your IDE version to the 2.2 (link).

Best Regards,

Alexis Andalon

0 件の賞賛
返信
2,896件の閲覧回数
w_lingjun
Contributor III

Hi Alexis,

Thank you very much for your reply.

Actually, I have uninstalled S32DS_ARM_v2.0 and install S32DS_ARM_v2018.R1, but still exist the error, the log as below. Today, I will try to update S32DS_ARM_v2.2 and test it.

I didn't modify the arp file, and I check the modified time is 2017/8/8, it is very strange.

Connection from "127.0.0.1" via 127.0.0.1
Connection from "127.0.0.1" via 127.0.0.1
PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read registers while part is running.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
Telnet server running on 127.0.0.1:51794
Searching for FreeRTOS Kernel Symbols...
pxCurrentTCB not found. FreeRTOS analysis not enabled.
PE-ERROR: Warning. Can't read memory while part is running. @0 (4 bytes)
Copyright 2017 P&E Microcomputer Systems,Inc.
Command Line :C:\NXP\S32DS_ARM_v2018.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.5.6.201805161649\win32\pegdbserver_console -device=NXP_KEx_S9KEAZ128M4 -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=500?

CMD>RE

Initializing.
Target has been RESET and is active.
CMD>CM C:\NXP\S32DS_ARM_v2018.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.5.6.201805161649\win32\gdi\P&E\supportFiles_ARM\NXP\KEx\freescale_s9keaz128m4_pflash.arp

Initializing.
Initialized.

;version 1.03, 06/02/2014, Copyright 2014 P&E Microcomputer Systems, Inc. All rights reserved. www.pemicro.com [ke_128k_pflash_ftmre_m0]

;device freescale, s9keaz128m4, pflash

;begin_cs device=$00000000, length=$00020000, ram=$20000000

Loading programming algorithm ...

WARNING - Selected .ARP file has been modified. CRC16 = $2AD1
Done.
Programming sequency is : erase, blank check, program, and verify {default}
CMD>VC
Command is inactive for this .ARP file.

CMD>EM
Command is inactive for this .ARP file.
Error Erasing flash of device
Error occured during Flash programming.

Best regards,

Sarah

0 件の賞賛
返信