Embedded Trace Macrocell (ETM) PCB Routing Tips

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Embedded Trace Macrocell (ETM) PCB Routing Tips

2,949件の閲覧回数
pgvoorhees
Contributor II

Hello Community,

We are planning on using ETM to aid in debugging but have found very few routing guidelines for the TRACE_D[0:3] and TRACE_CLK nets.

On the K22FX512, using a 120MHz core speed, What is:

  • The clock speed of the TRACE nets? Datasheet says the interface is limited to 50MHz but offers no guidance for determining the speed.
  • Is any particular characteristic impedance for the traces necessary?
  • Do the lines need to be length-matched?

Design guild-lines seem to be largely unavailable and the Kinetis datasheets are light on details for this particular functionality. Any help is appreciated. Thanks!

ラベル(1)
0 件の賞賛
返信
1 返信

2,625件の閲覧回数
pgvoorhees
Contributor II

The best reference I've found for this is the Segger J-Link/J-Trace manual.

J-Link Debug Probes | SEGGER - The Embedded Experts 

Chapter 17 (as of this post) called "Designing the target board for trace"

0 件の賞賛
返信