EZP Port issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EZP Port issue

1,155 Views
anna_palumbo
Contributor I

Hi,

i am using the micro MK22FN512, and the gpio EZP_CS is put to GND. In this condition on the power on the micro goes in the EZPORT mode. 

I have found a solution to avoid this behaviour -> disable the EZ register on the FOTP (0x40D) using the SPI protocol.

The question is: Can i send the right command sequence

* WRITE_ENABLE CMD

*ERASE THE SECTOR CMD (0x00)

* WAIT THE SE REGISTER IS SET

*WRITE_ENABLE CMD

*PROGRAM ADDRESS CDM (0X40D0

*WAIT THE SE REGISTER IS SET

if the EZP_CS is put to ground during the sequence? Or is it necessary handle it and have a falling edge before send a command?

Thank you,

-Anna

0 Kudos
Reply
1 Reply

1,088 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi Anna,

First, if you clear FOPT[EZPORT_DIS], chip will not enter EZPORT mode. You can't program FLASH at any time.
If you connet EZP_CS to ground, you can't send SPI command. "The negation of EZP_CS indicates that the current command has finished and resets the EzPort state machine, so that EzPort is ready to receive the next command."

Regards,

Jing

0 Kudos
Reply