Dynamically Adjusting the eDMA Destination Address K64F

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Dynamically Adjusting the eDMA Destination Address K64F

1,316 次查看
wildhorsemusic
Contributor III

Hello,

I'm trying to dynamically update the destination address on an eDMA channel to switch page buffers.  

I am using the K64F Freedom board to read an ADC channel.  The eDMA channel writes to a circular buffer using a modulo of 1024 (1 of 4 pages). I also use the Hardware Compare Mode of the ADC to fire if the ADC value is below a threshold.  As a rule, the ADC can fire prior to filling up the buffer and/or overflowing the modulo. When this happens, I want to switch buffer pages.  

Everything works except updating the eDMA DADDR register for the channel. After I update register with another page address, the channel goes back to the previous buffer (it appears to continue where it left off before the  

update).  I have read the Reference Manual, Section: 22.5.7 Dynamic programming.  Also, in Section: 22.5.5.2 Reading the transfer descriptors of active channels, it appears that the TCDn_SADDR, TCDn_DADDR, and TCDn_NBYTES registers are kept within the eDMA engine while the channel is active.  Does this mean that updating the hardware registers dynamically, won't actually change the DADDR  that is in process?

What is a work-around that I can use?  I tried clearing all of the registers for the channel.  I could use driver function that cancels the current transfer, but I have other channels operating on other things and it doesn't appear there is a way to cancel the transfer of a specific channel.

Thank you!

Duane

标记 (1)
0 项奖励
回复
1 回复

1,209 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi, Duane

There is an application for you to refer to. Please find AN4590 in www.nxp.com. I think it may useful to you.

Regards

Jing

0 项奖励
回复