Drivers for KEA-128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Drivers for KEA-128

3,637 Views
vignesh_vb_7
Contributor IV

Are there drivers for KEA-128?

7 Replies

3,186 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Vignesh,

- There is MSCAN driver for kea-128 chip :

Kinetis KEA128 StarterTRAK CAN Applications|Freescale

pastedImage_1.png

And if you use the KDS IDE, you can create PE project , then there are all of the basic driver about KEA-128 .

pastedImage_2.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,186 Views
vignesh_vb_7
Contributor IV

Hi Alice,

The Code Warrior IDE also has PE.The PE in KDE IDE and Code Warrior IDE are they both same?will the both PE generate same drivers or is there any changes in the PE that both of them are having?

0 Kudos
Reply

3,186 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello vignesh,

No, there maybe some difference .

And the majority is the same , while it hard porting one project from one IDE to another one .

SO if you use the PE , i recommend you direct use the IDE you want to use .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,186 Views
vignesh_vb_7
Contributor IV

Thank you Alice.Does the PE in KDS IDE has an advantage over the PE in CodeWarrior IDE ?

0 Kudos
Reply

3,186 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello vignesh, yes , the updates and support products in KDS are more than in CW .

Hope it helps

Alice

0 Kudos
Reply

3,186 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi vignesh balaji,

      Because the CW won't update the new kinetis product, the new kinetis product just be updated in KDS, then I suggest you use KDS.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,186 Views
kerryzhou
NXP TechSupport
NXP TechSupport


Hi vignesh balaji,

         Please refer to the attached KEA driver.

         Wish it helps you!

Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply