Drivers for KEA-128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Drivers for KEA-128

3,628件の閲覧回数
vignesh_vb_7
Contributor IV

Are there drivers for KEA-128?

7 返答(返信)

3,177件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Vignesh,

- There is MSCAN driver for kea-128 chip :

Kinetis KEA128 StarterTRAK CAN Applications|Freescale

pastedImage_1.png

And if you use the KDS IDE, you can create PE project , then there are all of the basic driver about KEA-128 .

pastedImage_2.png

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,177件の閲覧回数
vignesh_vb_7
Contributor IV

Hi Alice,

The Code Warrior IDE also has PE.The PE in KDE IDE and Code Warrior IDE are they both same?will the both PE generate same drivers or is there any changes in the PE that both of them are having?

0 件の賞賛
返信

3,177件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello vignesh,

No, there maybe some difference .

And the majority is the same , while it hard porting one project from one IDE to another one .

SO if you use the PE , i recommend you direct use the IDE you want to use .

Hope it helps


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

3,177件の閲覧回数
vignesh_vb_7
Contributor IV

Thank you Alice.Does the PE in KDS IDE has an advantage over the PE in CodeWarrior IDE ?

0 件の賞賛
返信

3,177件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello vignesh, yes , the updates and support products in KDS are more than in CW .

Hope it helps

Alice

0 件の賞賛
返信

3,177件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi vignesh balaji,

      Because the CW won't update the new kinetis product, the new kinetis product just be updated in KDS, then I suggest you use KDS.

Wish it helps you!


Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,177件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport


Hi vignesh balaji,

         Please refer to the attached KEA driver.

         Wish it helps you!

Have a great day,
Jingjing

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信