Does the freescale USB stack v4.1.1 support MK22FN processor?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does the freescale USB stack v4.1.1 support MK22FN processor?

777 次查看
solen
Contributor II

We are running a third party USB stack on our MK22FN Kinetis processor, and we are considering trying out the Freescale USB stack v4.1.1 since we have some problems with the third party stack.

But it is unclear to me whether the Freescale stack supports our target. Only K20 and K21 are listed among the development boards. But then, I would expect the USB block to be similar enough to be able to use this stack.

Happy for any feedback!

Thanks

Staffan

标签 (2)
0 项奖励
回复
1 回复

656 次查看
santiago_gonzal
NXP Employee
NXP Employee

Hello Steffan,

K22FN is fully supported in the Kinetis SDK 1.3 and you have several USB examples together with the USB Stack.

This stack included in the SDK 1.3 is the next version of the USB Stack 4.1.1.

2016-03-01 18_40_24-device.png

0 项奖励
回复