Does Developer's serial bootloader supports KE-02Z microcontrollers?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does Developer's serial bootloader supports KE-02Z microcontrollers?

ソリューションへジャンプ
1,557件の閲覧回数
ganeshramachand
Contributor IV

The application notes of Developer's Serial Bootloader in AN2295 states, "The microcontrollers supported by the developer's serial boot loader include 8-bit families HC08 and HCS08, and 32-bit families, ColdFire and Kinetis. New Kinetis families include support for K and L series. "

I would like to know whether it supports Kinetis E series controller too ?

To be specific I am using MKE02Z64VLD2 controller.

ラベル(3)
タグ(2)
0 件の賞賛
返信
1 解決策
1,367件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The AN2295 developer's loader is supported on the KE02 in the uTasker project:

http://www.utasker.com/kinetis/FRDM-KE02Z.html

http://www.utasker.com/kinetis/FRDM-KE02Z40M.html

and http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF

Also the KBOOT, SREC and IHEX loader modes can be used on the KE02.

Regards

Mark

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,368件の閲覧回数
mjbcswitzerland
Specialist V

Hi

The AN2295 developer's loader is supported on the KE02 in the uTasker project:

http://www.utasker.com/kinetis/FRDM-KE02Z.html

http://www.utasker.com/kinetis/FRDM-KE02Z40M.html

and http://www.utasker.com/docs/uTasker/uTaskerSerialLoader.PDF

Also the KBOOT, SREC and IHEX loader modes can be used on the KE02.

Regards

Mark

0 件の賞賛
返信