Does the Kinetis KL26 MCU support 'USB clock recovery' when using the IRC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the Kinetis KL26 MCU support 'USB clock recovery' when using the IRC?

2,582 Views
2743294708
Contributor I

I want to know, does the KL26 MCU support 'USB clock recovery' when using the IRC? I havn't find the information in 'KL26P121M48SF4RM'.

If supported, please give me the corresponding documents or example code projects that would accelerate the development.

Thanks.

Labels (2)
Tags (2)
0 Kudos
Reply
4 Replies

2,432 Views
mjbcswitzerland
Specialist V

Hi

The KL26 doesn't have IRC48M and so doesn't support crystal-less USB device.

The KL27 is needed instead.

Regards

Mark

- Better, faster, cheaper Kinetis developments for professional at: http://www.uTasker.com

0 Kudos
Reply

2,432 Views
2743294708
Contributor I

Dear Mark,

Thanks for your reply.

I have another question about this.

In the spec of KL26 chapter 3.8.1, there is a note says " The MCGFLLCLK does not meet the USB jitter
specifications for certification.
". Is there a method to ensure the MCGFLLCLK meets the USB jitter spec for certification when using the IRC?

0 Kudos
Reply

2,432 Views
mjbcswitzerland
Specialist V

Hi

The only way to ensure reliable USB operation and fulfill certification requirements is to use a crystal/oscillator source for the external clock or on the dedicated USB clock input.

It is impossible with MCGFFLCLK.

Regards

Mark

0 Kudos
Reply

2,432 Views
2743294708
Contributor I

OK.

It's clear about the question. Thanks.

0 Kudos
Reply