Does anyone know if configuring the FRDM-K64F FTM ( flexible timer module) to use an external clock that if the external clock period can be infinite.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does anyone know if configuring the FRDM-K64F FTM ( flexible timer module) to use an external clock that if the external clock period can be infinite.

2,144 Views
darringarrett
Contributor I

I need clock the FTM with an external clock that is driven off of a magnetic pickup mounted to a shaft of a motor.  This motor rotates from  equal to 0 rpm to 4000 rpm.

0 Kudos
Reply
2 Replies

1,885 Views
apanecatl
Senior Contributor II

In theory it is infinite, for your specific case I don't think you will face any problem using your clock source (4,000/60=66.66Hz).

0 Kudos
Reply

1,885 Views
darringarrett
Contributor I

Thanks Pedro,  I am mostly concerned about the ability of the clock to function from 0 rpm and up from there.  So if the FTM can be clocked at very low frequencies then I could use this board.

0 Kudos
Reply