Does NXP have a microcontroller with gigabit ethernet?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does NXP have a microcontroller with gigabit ethernet?

4,480 Views
rikardlarking
Contributor I

I need a device with following interfaces

1x Gigabit ethernet interface

1x CAN interface

2-4x RS232

1-2x SPI.

Possibility to have a bootloader (with ethernet)

Free development platform

Easy to implement a UDP-communication

Bonus:

mbed-support

ADC / DAC

SD-card

Best regards,

Rikard

Tags (1)
0 Kudos
Reply
1 Reply

2,772 Views
miduo
NXP Employee
NXP Employee

Yes, you may consider the i.MX6 SX device :

It has 2x Gigabit Ethernet with AVB-2x 10/100/1000 Mbps Gigabit Ethernet

(MAC) controllers (MII, RGMII) and two Flexible Controller Area Network (FlexCAN), 1 Mbps each.  

6 of UARTs and 5 of SPI. See detail from below link:

i.MX 6SoloX Family of Applications Processors|NXP

0 Kudos
Reply