Does NXP have a microcontroller with gigabit ethernet?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Does NXP have a microcontroller with gigabit ethernet?

3,988 次查看
rikardlarking
Contributor I

I need a device with following interfaces

1x Gigabit ethernet interface

1x CAN interface

2-4x RS232

1-2x SPI.

Possibility to have a bootloader (with ethernet)

Free development platform

Easy to implement a UDP-communication

Bonus:

mbed-support

ADC / DAC

SD-card

Best regards,

Rikard

标记 (1)
0 项奖励
回复
1 回复

2,280 次查看
miduo
NXP Employee
NXP Employee

Yes, you may consider the i.MX6 SX device :

It has 2x Gigabit Ethernet with AVB-2x 10/100/1000 Mbps Gigabit Ethernet

(MAC) controllers (MII, RGMII) and two Flexible Controller Area Network (FlexCAN), 1 Mbps each.  

6 of UARTs and 5 of SPI. See detail from below link:

i.MX 6SoloX Family of Applications Processors|NXP

0 项奖励
回复